AnsweredAssumed Answered

Stripline simulation using FEM

Question asked by ssaxena4 on Jan 20, 2014
Latest reply on Jan 21, 2014 by ssaxena4
Hi,

I am trying to simulate a stripline with FEM. I went through a tutorial. However, I getting the following error.

IndexError: list assignment index out of range
Traceback (most recent call last):
      File "/software/ads-2011_05_400/fem_scripts/sim.py", line 654, in main
  File "/software/ads-2011_05_400/fem_scripts/sim.py", line 532, in import_settings_and_simulate
    proj.ads_import()
  File "/home/ssaxena4/Research/HSpeed_Wireline/FEM_sims/simulation/FEM_sims_lib/dstrip_1in/layout/emSetup_FEM/proj.py", line 233, in ads_import
    waveguide.faces=[(part,part.faces()[0])]
IndexError: list assignment index out of range

  File "/software/ads-2011_05_400/fem_scripts/sim.py", line 658, in
main()
    simObject.import_settings_and_simulate(stop_after_project_creation)
    self.openOrCreateEMProProject(proj)
  File "/software/ads-2011_05_400/fem_scripts/sim.py", line 388, in openOrCreateEMProProject

And the simulation gets aborted. Can someone help tp debug the problem? I tried to simulate an example and that runs fine. But, the stripline which I created is an issue.

Thanks for the help.

Saurabh

Outcomes