I just upgraded our N9020A MXA from A01.24 to A14.03.
I'm having problems handling limit lines and antenna correction factors on this unit. Have followed http://cp.literature.agilent.com/litweb/pdf/5989-6126EN.pdf to the word, but there are no menu entries anywhere for editing correction factors. It's possible to load load correction factors from a csv file using the Recall Data (import) function, but the factors are removed when I use trace recall. After that it's impossible to reload the correction factor without perfoming a Mode Preset. It's impossible to know wheter the correction factors are loaded or not.
Anyone can help?
Thanks.
I'm having problems handling limit lines and antenna correction factors on this unit. Have followed http://cp.literature.agilent.com/litweb/pdf/5989-6126EN.pdf to the word, but there are no menu entries anywhere for editing correction factors. It's possible to load load correction factors from a csv file using the Recall Data (import) function, but the factors are removed when I use trace recall. After that it's impossible to reload the correction factor without perfoming a Mode Preset. It's impossible to know wheter the correction factors are loaded or not.
Anyone can help?
Thanks.
One of these is needed for amplitude corrections and limit line functions to be available
Best regards,
Mike