Hi.
Please how can i add a new rf transistor ( sp2 and non linear model) in the ADS's libraries?
Edited by: vodepam2 on Jun 7, 2014 3:23 PM
Please how can i add a new rf transistor ( sp2 and non linear model) in the ADS's libraries?
Edited by: vodepam2 on Jun 7, 2014 3:23 PM
For the s-parameter model you do not need to add the device to a library as ADS can access the .s2p file direct from the schematic. Just place an S2P symbol and assign the filename for the .s2p file and you will be able to do s-parameter simulation of the circuit.
The non-linear model though depends on the format and type of data that you have the non-linear model. Many different models are available and can also be entered directly in the schematic if required.