Is it possible to programatically set the eye boundary percentages? I think one possible way to do this would be to STOR/REC the scope setup, but I wanted, if possible, just to change the percentages directly.
I tried issuing :MTESt:MMARgin:PERCent and it didn't change the parameters I'm targeting. Specifically, I'm interested in the Eye Boundary percentages that can be accessed on the user interface like this: Measure->Setup & Info->Configure Meas...->Eye Boundary.
I'm thinking now maybe this is impossible to do without saving a state with the desired boundaries and switching to that. . .
Here is a command which should help set the mask margins programmatically for the 86100C.
+:MTESt:MMARgin:PERCent
+This command sets the amount of mask margin to apply to the selected mask.+
+
More details on the syntax are on page 242 below.
http://cp.literature.agilent.com/litweb/pdf/86100-90086.pdf
Let me know if this helps out.....
Regards,
John