When using the Object and Function Browser in Vee 7.0 and selecting AgilentPNA835X as a type library and anything as Class and members and then clicking on HELP I get "There is no help for xxx". Is there someway to get this function to work?
Thanks
Al Garvin
Thanks
Al Garvin
I see the same results for the PNA Object model help in both Vee 7.0 and 7.5. I expect the linkages from PNA COM Object Model to the Vee Environment help have not been generated or established. Until these linkages are generated (assuming they are ever generated) I recommend you reference the PNA COM Object model embedded in the PNAHelp.chm file. This file is downloadable directly to your PC via http://na.tm.agilent.com/pna/help/index.html
Note that for SOME of the PNA COM Object Class Properties, Methods, etc. there may be a small snippet of help information embedded in the Vee fx and object browser page. See attached and look for the text highlighted via the blue box.
I will also enquire with both my Vee and PNA colleagues as to what it would take to engage these linkages. If and when I hear a response I will let you know via this forum.
tsilchia.