Hi all
I m interesting to buy one synthesizer which has afrequency renge 80MHz,external trigger, infinitly-long random sequence, phase continuous and.... So I can find some same specification in Agilent 33600A Series Trueform Waveform Generators(33611A) but their manual isn't complete and I can't get for example about phase continuous,is there anybody who used this stuff before? if yes, how is it?
Thanks
I m interesting to buy one synthesizer which has afrequency renge 80MHz,external trigger, infinitly-long random sequence, phase continuous and.... So I can find some same specification in Agilent 33600A Series Trueform Waveform Generators(33611A) but their manual isn't complete and I can't get for example about phase continuous,is there anybody who used this stuff before? if yes, how is it?
Thanks
I have not used the 33600A waveform generator, but I did find the 33600A data sheet indicated on p19 for the Sweep Characteristics a footnote #12. The footnote is written on page 22, and states “12. All frequency changes are phase-continuous.”. This would indicate that it is phase continuous.
I hope this helped!