AnsweredAssumed Answered

Eval Agilent Vee: Barchart with error bar (confidence interval)

Question asked by JrV on Nov 23, 2013
Latest reply on Dec 4, 2013 by dBdetlef
Hello,

I am doing an evaluation of Agilent-VEE 
(last time use was in 1999, at that time HP-VEE).

Application:
I do a couple of measurements (for example a voltage). 
I calculate the mean and standard deviation.
Can I plot a barchart (mean) with a error bar (confidence interval) direct in Agilent-VEE at the end of the measurement.
We can export the data to excel, but this is not an option.

Any suggestions (example) are welcome.

Many thanks.

Regards,
J

Edited by: JrV on Nov 23, 2013 9:10 AM  

Outcomes