AnsweredAssumed Answered

How many link cables (1 or 2) to add front panel sampler access to 8720D?

Question asked by drkirkby on Aug 5, 2013
I want to add option 012 (front panel sampler access) to my 8720D. Agilent have declined to add it, since the instrument is obsolete and no stock is held of one cable. 

http://na.tm.agilent.com/8720/20ESupgrades.htm has the parts list needed to add option 012 to an 8720ES, one of which is an external link 08720-20098. That same part is needed for my 8720D. The quantity of that part is listed as 1, but am I correct in assuming two would be needed and so there is an error at http://na.tm.agilent.com/8720/20ESupgrades.htm

I'm trying to find out how practical it is to add option 012 myself, but knowing the number of cables needed would be a start! 

Dave  

Outcomes