Hello,
I am new user with the 2000-x series oscilloscope. I am having a query can anybody solve it.
I am using my this oscilloscope for getting current measurement in mobiles. So whenever my mobile is in idle mode, then power is utilized only at the time of paging. So whenever my mobile listen to paging channel some current is withdrawn so graph will show some fluctuation so i wants to calculate the average of that particular time when mobile wakes up. Is there any function present in this 2000-x series oscilloscope so that automatically i got the average time value of wake up. If there is any function present which automatically calculate average of time or i have to calculate it manually. if so then please help me out friends.
Thanks
Abhishek
I am new user with the 2000-x series oscilloscope. I am having a query can anybody solve it.
I am using my this oscilloscope for getting current measurement in mobiles. So whenever my mobile is in idle mode, then power is utilized only at the time of paging. So whenever my mobile listen to paging channel some current is withdrawn so graph will show some fluctuation so i wants to calculate the average of that particular time when mobile wakes up. Is there any function present in this 2000-x series oscilloscope so that automatically i got the average time value of wake up. If there is any function present which automatically calculate average of time or i have to calculate it manually. if so then please help me out friends.
Thanks
Abhishek
Al
Disclaimer: For more reliable response, you should consider calling your local Agilent Technical Call Center. The Agilent Forums are monitored on an "as available" basis, and aren't necessarily the fastest way to get technical questions answered.