AnsweredAssumed Answered

3 port s parameters from a 2 port network analyzer

Question asked by biff44 on Aug 13, 2013
if i have an 8722C, and need to make 3 port calibrated TRL measurements, like on a ferrite circulator, is there any softare available to do the math?

I can manually do the measurements by moving cables and using a 50 ohm load on the unused port, but i am not getting any calibration on the probe tips and 50 ohm load, since it is not part of the 2 port cal.  Was hoping some external software was available to do the magic.  

Outcomes