The PC5 processor comes standard on the N9010A EXA signal analyzer. It is a single core, 64-bit processor. If you would like to upgrade your EXA to have a dual core, 64-bit processor, you can purchase it with option PC4. Both of these processors are Win7 ready.
Please let me know if you have any additional questions. Best Regards, Scott
Yes, I have another question, I would like to upgrade processor and OS, my N9010A have PC1 processor card and firmware updated to A11.03. The right option for PC4 processor card and Windows 7 is N9094AK-PC4 & N9094AK-W7X, it is correct?
I found theses information for PC4 few month ago, it is correct: I7 processor dual core 64 bits 8 GB RAM Intel SSD 80GB (ssdsa2m080g2gc)
You are also correct about what you need to order. For your situation, you will want N9094AK-PC4 and N9094AK-W7X. Note that A.12 firmware is required for Windows 7. In the future, here is a good link to use as a reference to answer questions about what to order for Windows 7: http://www.home.agilent.com/agilent/editorial.jspx?cc=US&lc=eng&ckey=2290770&nid=-536902453.0.00&id=2290770
The PC5 processor comes standard on the N9010A EXA signal analyzer. It is a single core, 64-bit processor. If you would like to upgrade your EXA to have a dual core, 64-bit processor, you can purchase it with option PC4. Both of these processors are Win7 ready.
Please let me know if you have any additional questions.
Best Regards,
Scott