AnsweredAssumed Answered

Display goes off on certain settings

Question asked by tjh212 on Apr 19, 2013
Latest reply on Jun 18, 2013 by MikeM
When I use the following routine on a 8560 spec an, about 25% of the time the analyzer screen would disappear (including the grids), on the SP command or the VBW command.  Any ideas appreciated.

IP;
Wait for STB?; = 29 (commands done)
CF 1270000000 HZ;
Wait for STB?; = 29
SP 32000000 HZ;
Wait for STB?; = 29
RB 100000 HZ;
Wait for STB?; = 29
VB 10 HZ;
Wait for STB?; = 29
RL = -40 DBM;
Wait for STB?; = 29
LG 5 DB;
Wait for STB?; = 29
VAVG ON;
Wait for STB?; = 29
TS;DONE?;
TRA?;  

Outcomes