I am having a problem with an E4438 VSG.
If my PC has a network address of 192.168.1.1 /255.255.0.0 ( /16 )
and my 4438 has a network 192.168.2.1 / 255.255.0.0 ( /16 )
I can not communicate with the VSG.
If the two are on the same Class C network with a netmask of ( /24 )
they communicate fine.
It seems like the VSG is ignoring the Netmask.
Any thoughts?
-MikeT
If my PC has a network address of 192.168.1.1 /255.255.0.0 ( /16 )
and my 4438 has a network 192.168.2.1 / 255.255.0.0 ( /16 )
I can not communicate with the VSG.
If the two are on the same Class C network with a netmask of ( /24 )
they communicate fine.
It seems like the VSG is ignoring the Netmask.
Any thoughts?
-MikeT
In order for the E4438C to work, it need to be set as such -
PC network address of 192.168.1.1
E4438C network address 192.168.1.2 / 255.255.0.0 ( /16 )
Give it a try!