AnsweredAssumed Answered

8753ES no options problem

Question asked by Pulse.Analyzer on Apr 17, 2007
Latest reply on May 5, 2007 by Pulse.Analyzer
Hello,
  I haven't looked at it thoroughly yet but here's a brief description.

Port 2 while starting the calibration prior to a verification the traces were way off from expected.
With a short - the trace started at -30 dB then was peaks and valleys acros the span. Same thing with an open but started at -40 dB.
With a load on the port the max marker value is -70 dB.


My guesses without any further looking are no output or port two is kaput in some manner.

Looking forward to some ideas or known answers.

Tomorrow I'll start with a swap of port one and port two unless I see something here first.  

Outcomes