AnsweredAssumed Answered

Strange display behavior of E3648A

Question asked by guidow on Jun 15, 2014
Hi all,

I have objected some behavior of the PowerSupply E3648A which I, well, find somehow strange.

Normally the display shows Volts and Amperes of the selected / activated output. When I now change this display content to display both Voltage readings of Output 1 and Output 2 everything is fine as well. 

When I now change the voltage setting via the front dial, the display jumps back to the Volts - Ampere mode of Output 1. No chance to keep the display setting !

This is nasty as we run two separate circuits and need to watch Output Voltage to both circuits.

Am I missing some setting here ?

Many thanks,

Guido  

Outcomes