Thanks for the help with the previous problem, but now there is a different problem. The E8257D is an option 550 and when the software tries to run the high band adjustment it fails. I've noticed that when it runs through the -3dBm test it runs very quickly and the power meter will drop dramatically in the higher frequencies (usually a drop between -10 or -11dB above 30GHz), but when the next to tests (-13dBm and -18dBm) run, they are much slower and show no significant drops. I've run something similar by hand and have not seen any drops that badly. The equipment being used switches up, I consistently use the 8487A power sensor, but I switch between the E4419B and the N1914A power meters (same problems with both meters).
Our support team will require some information from you. Referenced tools are attached.
• Can you send the Install.log file C:\Program Files\Agilent TME\Output\Install.log
• Can you send the Application's ErrorLog.txt file C:\Documents and Settings\All Users\Application Data\Agilent Technologies\Test Management Environment\Output\ErrorLog.txt
• Can you create and send a Jedix.jdr file of the test that failed/aborted? You will need to re-run the test with the Jedix Recorder running. This IO log can help us to see where in the test the error is occurring. (See process- attached)
• What are the UUT's Model & Serial number and Options? *If you can create a TME report and send it showing this info that is recommended.*
• What do you mean by Failing the PLA adjustment? Is the test aborting or completing with a “fail” status?
Thank you -
Edited by: tabbott on Apr 23, 2014 11:43 AM