AnsweredAssumed Answered

Problem to add reference IO librairy (COM) on VBNET

Question asked by ritong74 on Oct 22, 2014
Latest reply on Oct 22, 2014 by lhornburg
i install "io librairy 16.3"
I have a windows form vb net application and when i want to add reference librairy agilent under VS2010 i have this error :

Impossible de déterminer les dépendances de la référence COM "AgilentRS232Lib". Erreur lors du chargement de la bibliothèque/DLL du type. (Exception de HRESULT : 0x80029C4A (TYPE_E_CANTLOADLIBRARY
Le composant référencé 'AgilentRS232Lib' est introuvable.      


It's the same error for all agilent library i select.
Somebody have any idea of the problem ?


Thanks  

Outcomes