AnsweredAssumed Answered

Can't install AgilentRFPowerMeter 3.7.2.0 Driver

Question asked by iviaryjane on Oct 21, 2014
Latest reply on Oct 26, 2014 by eirp_inc
When I try to install driver_ivi_AgilentRFPowerMeter_3_7_2_0.msi (taken from the Agilent site) I receive two errors. 

The first pop-up says, "Another driver for this instrument is already installed.  You must uninstall the other driver first".  Then the second pop-up says, "AgilentRFPowerMeter IVI Driver 3.7.2.0 setup ended prematurely because of an error.  Your system has not been modified.  To install this program at a later time, please run the installation again."

I have looked at the installed programs in "Programs and Features" and poked a few other locations on my computer, and do not see anywhere that this program is installed anywhere.

I also tried installing IOLibSuite_16_3_16603.exe, as I was instructed that also having NI MAX on my system could be causing a conflict.  

Any ideas of what I can do?  Thank you so much in advance!

MJ

Attachments

Outcomes