I have a 33120A ARG gen, Agilent Intuiu.Link Waveform editor(v1.6.0). I have a .csv file that loads OK to the editor.
I need to load the waveform to one of the non-volitile memories. The only way so far I can download is to the volitile memory. I then am unable to save it to one of the three non-vol memories (it works until you power cycle, then it's gone). Is there a way to load it directly to one of the non-vol memories from the editor? I wants a named memory, teh 33120A has numbered memory locations.
I need to load the waveform to one of the non-volitile memories. The only way so far I can download is to the volitile memory. I then am unable to save it to one of the three non-vol memories (it works until you power cycle, then it's gone). Is there a way to load it directly to one of the non-vol memories from the editor? I wants a named memory, teh 33120A has numbered memory locations.
when you send file to 33120A, you have 2 choices, VOLATILE or MEMORY NAME, if you enter a name ("test" for example), memory will be non-volatile. I tried that on my 33120A with sucess, I used Agilent IntuiLink Waveform editor v1.6.0, 33120A revision 5.0-2.0-1.0.