AnsweredAssumed Answered

antenna S parameter measurements

Question asked by rsharp on Aug 15, 2006
Latest reply on Oct 27, 2006 by Wai
I am planning on renting an E5062A analyzer for doing some S parameter measurements on a specialized antenna.  However, I have not used a network analyzer yet and have been reading literature and listened to a web cast on your analyzer.  One of the biggest questions I have is probably simple.  Your analyzer has N port connections on it and the DUT has SMA connectors.  I assume that I need to purchase Male N to Female SMA connectors to be able to match the DUT, but which calibration set should I get?  The 85033e or the 85032f?  I am not sure if I will need to calibrate the unit with the adapters on the unit or not?  

Outcomes