AnsweredAssumed Answered

DMM trigger operation control from Benchvue

Question asked by edel on Jun 12, 2014
Latest reply on Aug 7, 2015 by w0dz
Hi,
I'm wondering if you can advise about some benchvue functionality?
I am using benchvue to remotely control the 34410A DMM. 
I cannot find a way of controlling the capture mode so that each sample is captured in response to a trigger. This was possible with the web interface (which has stopped working for me); I could set the data logger to capture a series of e.g. 10 samples on consecutive external triggers. This was useful for manual testing.
The benchvue software appears to be limited to timed captures only. Is this the case?
I can set up the DMM from the frontpanel to acquire a sample on each trigger but is there any way of logging more than 1 sample captured with this method?

Edel  

Outcomes