AnsweredAssumed Answered

PNAX Cal All Phase Correction Toggling issue

Question asked by rok on Jun 2, 2014
Latest reply on Jun 10, 2014 by rok
Hello,

I am using A.09.90.09 firmware on the Windows XP version of the PNA-X.
I was using the 'Use Receiver Characterization Calset' option during the 'Cal All' process, selecting 1 of the Tier 1 calibrations performed using a comb filter generator.. This caused the next screen titled 'Calibration Attenuator Settings' to have the 'Source Attenuator' section to be grayed out. (See attached). The problem I am encountering is that when I switch back the 'Enable Phase Correction' setting back to 'False',  in the next screen, the 'Source Attenuator' section is still grayed out! My question is how to fix it so that I can enter values in the 'Source Attenuator' section again when the 'Enable Phase Correction' setting is set 'False' from a prior state of being set to 'True'. 

Best regards,
rok  

Outcomes