AnsweredAssumed Answered

SOLVED Get data from DVM 3458A using subsampling

Question asked by PacoLopez on Jun 2, 2014
Latest reply on Jun 2, 2014 by PacoLopez
Hello,

After long time using VEE to capture signals from a 3458A, we decided to use C# and recreate the same functionallity we had in our VEE application. I tried to create a function that programs the multimeter to work in subsampling mode, cause the signal we monitor is in the uS range.
I have been searching information about reading binary block of int16 using the libraries, but I couldn't find any information, all the examples use the NRDGS, is is possible to read the values using the VisaComLib in C#?  
I have attached the screenshot of the VEE function that setups the multimetera and the VEE function that we use to read the data. 

Thanks in advance,

Paco

Edited by: PacoLopez on Jun 10, 2014 11:57 PM

After some time trying several ways to read the data back from the DVM, I found how to do it....by myself

Edited by: PacoLopez on Jul 9, 2014 12:49 AM  

Attachments

Outcomes