Using the BenchVue Data Manager, you can import data logs previously stored from the Agilent DMM Connectivity Utility software. From the Data Manager sheet in BenchVue, click the "Import Data Logs" button to navigate to the desired location containing the data log from the Connectivity Utility software. By default, data logs are stored in the following directory from the Connectivity Utility software:
C:\Users\\Documents\Agilent\Agilent Digital Multimeter Connectivity Utility\DataLogs\
If the data log is located in a folder on your local computer, BenchVue will add a reference to that folder in the Data Manager list.
If the data log is located on a network drive or an external hard drive, BenchVue will copy the data log to the "My Documents" folder on your local computer, in instrument-specific folders. For example – C:\Users\\Documents\Agilent\BenchVue\Digital Multimeter\Data Logs\. Once the data log folder is copied, BenchVue will add a reference to that folder in the Data Manager list.
Depending on the size of the stored data log, an import operation could take some time to complete.
C:\Users\
If the data log is located in a folder on your local computer, BenchVue will add a reference to that folder in the Data Manager list.
If the data log is located on a network drive or an external hard drive, BenchVue will copy the data log to the "My Documents" folder on your local computer, in instrument-specific folders. For example – C:\Users\
Depending on the size of the stored data log, an import operation could take some time to complete.
Hi daveh,
I'm not able to import file(csv) into DMM.
Could I send you my File then you can check if its correct?
Thanks in advance.
Hervé