AnsweredAssumed Answered

N9020A MXA Signal Analyzer in remote mode using LAN

Question asked by horacio on Jun 12, 2014
Latest reply on Jun 25, 2014 by tjzeta001
Hi there!!!

Im so confused, i have a N9020A MXA Signal Analyzer and i wanna connect the analyzer in LAN for example for 2 or more computers and use the analyzer at the same time with the option of remote mode.
My question is: is this possible?
Can I connect the analyzer in remote mode for 2 or more computers and use it at the same time? the idea is, using this analyzer in a classroom for all the students at the same time to teach them how use the analyzer, but every student may use the analyzer individual from their computers and make some test to learn how use the analyzer.  

I did the romote mode with only one computer and works well, I wanna use for 2 or more computers. i heard i need  a switch but, is possible?

I hope someone can help me
thanks  

Outcomes