AnsweredAssumed Answered

Execute Program simple question

Question asked by wangyiliu99 on Jun 23, 2013
Latest reply on Jun 25, 2013 by Mike
Hi, all

sorry to bother again.

One simple question about the execute program in VEE.

(1) *.exe needs certain time to do the data process, 
would it okay just to connect the execute program block sequence pin to the following blocks.
So only after the data process by exe is complete will VEE continue processing to the next step.

Or, I need to add some delay time in between the sequence pins?

(2) When "wait for prog exit" is set to "Yes", after the program exit, "0" will be propagated to the "Exit code",
can I use this exit code 0 to help with the flow control, say, connect that to the sequence pin of the next block?

Sorry for the naive question, I do appreciate your great help.

Yours,
Yiliu  

Outcomes