I have an Agilent InfiniiVision 2000 X-Series Oscilloscope. One channel is not displaying any signal. how can i fix this? If the channel is damaged can i replace it?
This is not user-repairable, probably. If it's in warranty, get it to Agilent. If it's not in warranty, then either fix it or replace it.
Al
Disclaimer: For more reliable response, you should consider calling your local Agilent Technical Call Center. The Agilent Forums are monitored on an "as available" basis, and aren't necessarily the fastest way to get technical questions answered.
I assume that the channel button is lit up. Sometimes the trace position is off the scale in which case, on the left side of the screen, you will see the channel number, next to it an up or down pointing arrow and the letter T. If that the case, just push the channel position knob.
It happened to me once and I almost posted the same topic on this forum.
Al
Disclaimer: For more reliable response, you should consider calling your local Agilent Technical Call Center. The Agilent Forums are monitored on an "as available" basis, and aren't necessarily the fastest way to get technical questions answered.