Good morning,
I am currently looking for a method to inject noise patterns onto CMOS power rails and wanted to know if any Agilent Supplies offered this option. I need something that can be controlled via Linux and Windows drivers (or even better, driverless via Serial/Network/whatever) to automatically inject arbitrary noise patterns and levels on top of a clean DC rail.
Thanks for the help,
Chuck
I am currently looking for a method to inject noise patterns onto CMOS power rails and wanted to know if any Agilent Supplies offered this option. I need something that can be controlled via Linux and Windows drivers (or even better, driverless via Serial/Network/whatever) to automatically inject arbitrary noise patterns and levels on top of a clean DC rail.
Thanks for the help,
Chuck
What are the required voltage and current as well as the frequency of the noise? If it is low power and low frequency then you might be able to do something. If it is higher power then you might want to try something like this blog post suggests: [http://gpete-neil.blogspot.com/2012/09/simulating-power-supply-noise.html].
Thanks.