AnsweredAssumed Answered

More additional Coplanar model available in the Eagleware library?

Question asked by tchang on May 30, 2014
Latest reply on Jun 27, 2014 by dan.peabody
Are there any additional coplanar models available for the Genesys 2012?  The one that I'm particularly interested is the differential coplanar with ground plane model, but I'm also interested in multiple coupled coplanar lines with ground plane (such as the effect of the gap to the adjacent ground for the outer lines).  

Outcomes