AnsweredAssumed Answered

measure equation

Question asked by victor007 on Jun 18, 2013
Latest reply on Jun 19, 2013 by sdgrant
Hi,
I am newbies in ADS and seraching for help in this forum.
I have read the user manual on measurement expressions. 
I found that some of the expressions I can used for my simulation. Now I can use max(out) to find the maximum output of my simulation data.
The problem here is I don't understand whether I can return the value of frequency for single point in the graph.
Example:
I wan to know when the frequency value when the output is -3dB. I don wan to manual read it from the bode plot.
Is it possible ?

Regards,
Victor007  

Attachments

Outcomes