Can someone confirm that the phase control function of the 33522 generators has a resolution of only 100mdeg and not 1mdeg as in the 33220/33250 units thanks
We just released a new firmware rev 2.09, that let's you set phase in degrees, radians, or time. Simply change the default units from the Units menu (front panel) or with the UNIT:ANGLe command. You can also select the unit when setting the phase via the front panel or remote interface.
If setting the phase in terms of time, you get far more resolution than you did previously with degrees. It also now lets you set the phase in terms of degrees down to 1mdeg.
We just released a new firmware rev 2.09, that let's you set phase in degrees, radians, or time. Simply change the default units from the Units menu (front panel) or with the UNIT:ANGLe command. You can also select the unit when setting the phase via the front panel or remote interface.
If setting the phase in terms of time, you get far more resolution than you did previously with degrees. It also now lets you set the phase in terms of degrees down to 1mdeg.
The firmware can be downloaded here:
[http://www.home.agilent.com/agilent/software.jspx?ckey=1974550&lc=eng&cc=US&nid=-33134.1026944&id=1974550]