AnsweredAssumed Answered

N3383A support of E series power meters

Question asked by mirek on Jan 22, 2014
Latest reply on Jan 22, 2014 by jvall
I am traing to use E4418A powe rmeter with N3383A Network Analyzer. The Network Analyzer do not recognize that model. I have on that Newtok Analyzer Agilent IO 16.3, and it recongized the E4418A in there.
I have no problem to perform source power leveling using the old 437B power meter. 
The firmware on the Network Analyzer is A.04.87.01. The NA help menu for power meters have some statement that the E series power meter can execute up to 200 reading, so I asume that that firmware support the E seriaes power meters.
 
Any reason why it do not work?  

Outcomes