AnsweredAssumed Answered

Fieldfox charger

Question asked by theamberco on Dec 29, 2013
Latest reply on Jan 13, 2014 by theamberco
Hi, the fieldfox manual say the charger should be a 15V @ 4A. 60W.
The back of the N9912A say can be used to 19V.
The unit came with a 19V @ 3.15A.  59.85W.
Since the power is about the same, can that charger be used on the Fieldfox?
Did you shipped any units with the 19V. power supply?

Mike.

Edited by: theamberco on Dec 29, 2013 1:40 PM  

Attachments

Outcomes