So my question here is do i need to turn the option on after i install the hardware or does the instrument automatically detect the presence of the attenuator ? i was looking through the manuals and could not find any hints , i also scrolled through the special function menues to see if there is any service menue to enable the attenuator but with no sucess !
any input on this ?
You will need to turn the option on and there is a sub menu that will allow you specify which attenuator your using. The A series used a 90db step atten and the B series used a 110 db step attenuator. This post is so old I assume you already got this worked out if not. you can email me for more info. service@teplus.com