AnsweredAssumed Answered

need help!!variable frequency problem

Question asked by boon on Dec 28, 2009
Latest reply on Jan 29, 2010 by mescaline
I'm the user of Agilent’s E4980A precision LCR meter. Now i 'm doing the final year project that to develop a friendly-user software so that the user can operate the instrument through the computer.So far i had successful to connect and get the result from the instrument by using the visual basic programming language.However i failed to set the variable frequency.As we need to key in the value of frequency into the SCPI command ":FREQ:CW <numeric>" only can change the instrument's frequency.Hence,is it got other ways to solve this problem?


Thank!
boon  

Outcomes