AnsweredAssumed Answered

How to create a two channel coupled frequency sweep?

Question asked by Patrick on Aug 2, 2012
Latest reply on Aug 10, 2012 by cldiller
I want to create two outputs on both channels of my agilent 33522A function generator to synchronously sweep but at different frequencies.

*example:*
CH1
sine wave
start freq: 50Hz
stop freq: 200Hz

CH2
square wave
start freq: 4.15kHz
stop freq: 16.6kHz

I've tried using the sync output, but I'm unable to set the frequency coupling ratio. Is this possible?  

Outcomes