Hi,
I am having Agilent Technologies Low-Profile Modular Power Systems mainframe, N6700B with DC power module N6732B. Appreciate your advice & help on below items:
1. How to enable the measurement function under Meter key? The measurement is displayed as grey in italic, unable to use the function.
2. How to set the current & voltage measurement decimal place at Front Panel Display. Currently, the voltage & cuurrent measurement at Front Panel Display is only showing 3 and 4 decimal places respectively.
Thanks.
-SY
Let me take a stab at the questions.
1. The measurement function is alway enabled on this unit. From the user's end, I don't think there is anything that needs to be done to enable this feature. Perhaps you can take a quick picture of fornt panel showing this and I can help you debug it.
2. As for the decimal place, there isn't a way to change the decimal place of the displayed values. I spent a bit of time looking for it today but I couldn't find a setting over the front panel. Also from my previous experience, I don't recollect that being something that can be control by the user.
Steven