AnsweredAssumed Answered

Checkout the Built-in Help Feature of the 53200 series frequency counters

Question asked by jdwindrvr Employee on Oct 19, 2012
This video reviews the help system included with the Agilent 53210A, 53220A and the 53230A Frequency Counters. You can quickly get information about the firmware revision or front panel button. Six different languages are available.
Video: http://www.youtube.com/watch?v=Ct50_7CjKt0

For more information:
http://www.agilent.com/find/53210A
http://www.agilent.com/find/53220A
http://www.agilent.com/find/53230A  

Outcomes