Have you read/done this from VEE's Readme-file? Dont know if also this error can occur...
When using Agilent VEE 9.2 in Windows 7 64-bit using WOW64 emulator, please be informed of the following limitations:
1. Error running Agilent VEE program or Agilent VEE runtime program containing MATLAB scripts
If you are running Agilent VEE program (.vee) or Agilent VEE runtime program (.vxe) containing MATLAB scripts for the first time, the error dialog "Matlab engine could not be started" may be prompted. Steps to fix this:
Go to Start | Run and type 'secpol.msc'. In the prompted dialog, navigate to Local Policies | Security options. Set the value of User Account Control: Run all administrators in Admin Approval Mode to Disabled. Restart system and login with administrator privileges. Run the Agilent VEE program or Agilent VEE runtime program again and it should work fine. Repeat steps 1-4 with the value of User Account Control: Run all administrators in Admin Approval Mode set to Enabled. If step 6 is not performed, Standard User may not be able to launch Agilent VEE.
Sorry, something is wrong?
http://s017.radikal.ru/i438/1110/85/1b11c2b66f81.jpg
When using Agilent VEE 9.2 in Windows 7 64-bit using WOW64 emulator, please be informed of the following limitations:
1. Error running Agilent VEE program or Agilent VEE runtime program containing MATLAB scripts
If you are running Agilent VEE program (.vee) or Agilent VEE runtime program (.vxe) containing MATLAB scripts for the first time, the error dialog "Matlab engine could not be started" may be prompted. Steps to fix this:
Go to Start | Run and type 'secpol.msc'.
In the prompted dialog, navigate to Local Policies | Security options.
Set the value of User Account Control: Run all administrators in Admin Approval Mode to Disabled.
Restart system and login with administrator privileges.
Run the Agilent VEE program or Agilent VEE runtime program again and it should work fine.
Repeat steps 1-4 with the value of User Account Control: Run all administrators in Admin Approval Mode set to Enabled.
If step 6 is not performed, Standard User may not be able to launch Agilent VEE.
O-ops! I have never read Readme...
Thank you very much!