AnsweredAssumed Answered

Issue with PNA

Question asked by DavidC on Sep 28, 2012
Latest reply on Oct 3, 2012 by DavidC
Have brought in a  N5230A network analyzer that the GPIB Settings have been changed.  There is no internal gpib interface configure to control the instrument from the internal windows. The external GPIB is set to 7xx address with a duplicate at 14xx. The io config has a GPIB0 and GPIB1 instead of HPIB7 with the gpib0 set to address 7, and GPIB1 set to 33. Is there a way of resolving this issue with out doing a restore?

-David  

Outcomes