AnsweredAssumed Answered

Improving Measurements for Battery Drain Current Measurements in Save Modes

Question asked by paulf on Oct 18, 2012
Improving Measurement Accuracy for Battery Drain Current Measurements During Power Saving Modes

Maximizing battery run-time for many wireless devices requires accurate measurement of low-level current drain during power-savings modes. Because of the long duration of these modes, they often consume more power than the higher level but infrequent active modes. Agilent Technologies provides a one box solution that can power a wireless device and capture the total current profile. Analyzing the profile data allows design changes to be characterized quickly.
Video: http://www.youtube.com/watch?v=KBqEx1KqL8E

For more information on the N6705B DC Power Supply Mainframe see: http://www.agilent.com/find/n6705

Also see N6781A DC Power SMU Module for additional details:
http://www.agilent.com/find/n6781

Information on the software shown in the video can be found:
http://www.agilent.com/find/14565  

Outcomes