Hi to all.
We have an HP 83631B which has showed a problem. As a first step in order to fix it we are trying to use the service support software and do the adjustments. Unfortunately the two disks accompanying the source, as well as our backup set, are damaged. I tried to locate the software here, but I can't find it anywhere. Could anyone please help me with that? Thanks in advance...
George
We have an HP 83631B which has showed a problem. As a first step in order to fix it we are trying to use the service support software and do the adjustments. Unfortunately the two disks accompanying the source, as well as our backup set, are damaged. I tried to locate the software here, but I can't find it anywhere. Could anyone please help me with that? Thanks in advance...
George
I am the admin who relocated this post to the Network Analyzer Forum as the Agilent 83631B is a dedicated source optimized for use with Agilent 8510 systems.
Unfortunately, the Agilent Signal Generator division did not support this obsolete source so I do not have access to the materials requested.
I'll see if I can get someone to assist from the Agilent Network Analyzer division (they support Agilent 8510 systems).
Sorry for the back and forth -
My internal tool says the part is available - the link I provided you says it is not (sorry - that was not what I expected).
To anticipate any more run around - I called the following number to be sure I am pointing you in the right direction. I am assurred the folks here will listen to you and try to help.
Please call Agilent repair & calibration at 1 800 829-4444 Press #, then 1
They should be able to verify part availability, pricing, or repair instructions.
I sure hope the path gets easier for you.
Regards -
I am not sure what the problem is. I have been scrabbling within manuals, application notes and the internet for the past two days, not finding a solution. I only suspect that some parameters are not correct during the migration (even though I have tried with the CONFIGURE statement to approximate the HP Basic / 9000 environment, with no success either). Has anyone been confronted with a similar problem?
PS. I am not sure whether this is the right place to post such questions, but I have placed it here since it is related to our source and I also could not find a more related (sub-)forum.
What problem are you having with the 83631?