AnsweredAssumed Answered

vrf Identifing E Series Sensor models on HP/Agilent E4418 or E4419 Power Meters

Question asked by VRFuser on Sep 8, 2008
Latest reply on Sep 8, 2008 by VRFuser
Why not using the Windows integrated taskplaner for this ?
detlef

-----Ursprüngliche Nachricht-----
Von: Voltz, Gary [mailto:gary.voltz@AirservicesAustralia.com]
Gesendet: Dienstag, 9. September 2008 01:30
An: VRF
Betreff: RE: [vrf] [VRF] VeeServiceManager not working on first start


I had a problem with trying to update Antivirus files at boot-up from a Server on an isolated LAN. If the program ran after boot up was complete, there was no problem, so I decided it must be due to the intense process of booting up, therefore I needed a delay before calling the update program.

So I wrote a little program that uses .Net "System.threading.thread.sleep(mSec)".   I used Visual Basic Express 2008, however I'm sure it could be done in VEE as well.  I used 120000 milliseconds (2 Minutes) to give the boot-up process enough time to complete before for calling the update program.

Shawn, I think this would be right up your alley.  It'd be nice if it could use a command line input to include the path and filename of the program to run, to create multiple startup shortcuts if more than one program needs to be delayed, or a text file containing the programs to start.

Cheers,
Gary


Gary Voltz
Technical Officer (SASTO4)

Test Equipment Maintenance and Calibration Centre (TEMACC)
Facilities Management Services
Technology and Asset Services
Airservices Australia

E-mail: gary.voltz@airservicesaustralia.com
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Airservices Australia
Ph 1300 301 120       (within Australia)
   07 3886 3382
Ph +61 7 3866 3382    (outside Australia) 
Fax +61 7 3866 3531
www.airservicesaustralia.com
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

CAUTION: This e-mail is confidential. If you are not the intended
recipient, you must not disclose or use the information contained
in it. If you have received this e-mail in error, please tell us
immediately by return e-mail and delete the document.

Airservices Australia does not represent, warrant or guarantee
that the integrity of this communication is free of errors, virus
or interference.

-----Original Message-----
From: Shawn Fessenden [mailto:shawn@vrfarchive.com]
Sent: Tuesday, 9 September 2008 6:50 AM
To: VRF
Subject: RE: [vrf] [VRF] VeeServiceManager not working on first start

> The problem occurs only on the first start after rebooting.

Occam's razor1: Is the service set to start type "Automatic" instead of "On Demand"? May require dependent services (COM comes to mind). Check System log to find services that don't start for one reason or other.

Occam's razor2: Boot is an intense process. Maybe VeeSm.exe needs more time to start after the desktop appears?
-SHAWN-


Der Inhalt dieser E-Mail (inkl. aller Anlagen) ist vertraulich und ausschließlich für den Adressaten bestimmt. Jede Art der Verbreitung, Nutzung oder Vervielfältigung ist untersagt. Sollten Sie diese E-Mail irrtümlich erhalten haben, informieren Sie bitte sofort den Absender und löschen die E-Mail.

Unternehmensangaben der Gesellschaften mit Sitz in Deutschland:

Pilkington Holding GmbH, Haydnstraße 19, 45884 Gelsenkirchen
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 8997
Geschäftsführung: Dr. Clemens Miller (Vorsitz), Jochen Settelmayer, Thomas Kretschmann, Robert Hales
Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Deutschland AG, Haydnstraße 19, 45884 Gelsenkirchen         
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 2707
Vorstand: Dr. Clemens Miller, Jochen Settelmayer
Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Automotive Deutschland GmbH, Otto-Seeling-Straße 7, 58455 Witten
Sitz: Witten, Amtsgericht Bochum HRB 8443
Geschäftsführung: Thomas Kretschmann
Vorsitzender des Aufsichtsrates: Jochen Settelmayer

Bauglasindustrie GmbH, Hüttenstraße 33, 66839 Schmelz / Saar
Sitz: Schmelz / Saar, Amtsgericht Saarbrücken HRB 52020
Geschäftsführung: Manfred Ebbers


---
You are currently subscribed to vrf as: hua_jing@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes