AnsweredAssumed Answered

Network analyser HP8753D _ for one special measurement

Question asked by luoma on Apr 23, 2008
Latest reply on Apr 23, 2008 by luoma
hello everybody interested about Microwave...

It is the first time i come here, i hope my question is not too difficult and will have a rapid answer.

my question is about one particular measurement using the Network analyser HP8753D  . 

My boss told me that it seems to be possible using the Network analyser HP8753D to do the following measurement...

...Is it possible  to see   the gain variation of a DUT against the input power .
and the phase variation of a DUT against the input power.
The network analyser change himself the input power in one range i already insert

So How to see this? ( if it is possible with this network analyser) and how to do?


1) I would like to see the graph  : gain (Y) against input power (X) (for example from -15 dbm to -5 dBm) 

2) I would like to see the graph  : phase (Y) against input power (X) (for example from -15 dbm to -5 dBm) 


3)And how to tune the input power if i want another range of input power ( for example -30 to 0 dBm )

thanks for your help  

Outcomes