AnsweredAssumed Answered

Changes to Std Output module used with the 66000A

Question asked by carlp on Oct 16, 2012
This Video describes the changes to the DC Output connector assembly P/N 5060-3386 internal Printed Circuit Boards.
The 66000A Main Frame is stand alone. 6610XA Modules must be installed in the Mainframe. The Output connector assembly is required to connect the modules to the Device Under Test (DUT) . (cp)

Video: http://www.youtube.com/watch?v=1he6mGSDTnM

For more information:
http://www.agilent.com/find/66000  

Outcomes