Hello all,
I couldnt find the scpi command to enable the internal mixer("up conversion" in menu ) in scpi command brochure.
Could you help me please??
I also wonder if we can see the scpi commands that are sent when we press buttons on the control gui in the internet explorer?
Thank you,
I couldnt find the scpi command to enable the internal mixer("up conversion" in menu ) in scpi command brochure.
Could you help me please??
I also wonder if we can see the scpi commands that are sent when we press buttons on the control gui in the internet explorer?
Thank you,
You can find the command from the instrument help key. Here is an example: E8257D press: Frequency-> Help -> Freq Start: should see the command [:SOUR]:FREQ:STAR
The control gui in the internet explorer is not viewable.
Hope this helped -