AnsweredAssumed Answered

E5071C with 85024A probe to perform in-circuit measurements

Question asked by thomas9003 on Jul 11, 2012
Latest reply on Aug 8, 2012 by castellanosjoseg
Hi,

I need to measure my DUT (attached) which are RF Modules for 2.4GHz band and 5GHz band. 

I'm designing Bluetooth modules for Home Theatre systerm.

I'm using E5071C for my in-circuit measurement. 

The parameters I want to measure are mainly VSWR, S-parameters, etc.

Is 85024A High-Frequency Probe, 300 kHz to 3 GHz the right tool for measurement?

Can I use N1021B 18 GHz Differential TDR/TDT Probe Kit on E5071C?  

Attachments

Outcomes