Over a year ago I wrote a data collection program on a Trial version of VEE (6.0 I think). The trial has since expired and we need to run the program again; therefore we purchased VEE Express 9.2. When trying to open the old data collection program, I get the following error:
I have checked for the driver and it does exist in the panel driver section of the advanced instrument properties pop up. I also know that the scope we are using is connected to ther computer as the Agilent connection expert can see it. I know only of the following problem, the driver is for an 4339A meter and we are using a 4339B meter. However this setup worked when using the older trial version of VEE.
Your thoughts/advise would be greatly appreciated. Thanks.
Your thoughts/advise would be greatly appreciated. Thanks.
If possible, try to use the same alias you used for your initial trial.