In a micro strip filter design i got a structure like a Tee with a bent i.e., a Tee which has 2 horizontal arms and a vertical arm. One of the horizontal arm and the vertical arm are of same dimension 1.2 mm and the other horizontal arm is 3 mm. But the designed filter looks like it has a bent rather than a Tee's step change. Using ADS how to implement such a 3 arm structure?