AnsweredAssumed Answered

Does the PNA-X N5242A Sweep Time include overhead time?

Question asked by dedenne on Jul 9, 2012
Latest reply on Jul 11, 2012 by Dr_joel
I have the PNA-X sweeping in CW Time with a sweep time of 10.714ms.

The following commands are sent to read a marker.

SENS:SWE:MODE SING:*OPC?
CALC1:MARK1:Y?

It takes about 33ms to complete the two reads.  Is this overhead time that isn't included in the sweep time?

I'm using LabView.

Thanks.  

Outcomes